FB#.P

Description

This parameter is the 64 bit position of the feedback device. The position is given in counts. The parameter takes actual feedback position (with resolution specified in FB#.RES ) and converts it into a format of 32:32.

  • For rotary feedback, the upper 32 bits represent the number of motor turns and the lower 32 bits represent the position within one turn.

  • For linear feedback, the upper 32 bits represent the number of motor pole-pairs and the lower 32 bits represent the position within one pole-pair distance of the motor.

Example

Rotary feedback position = 542,456,123,450 or 0111 1110 0100 1100 1110 0111 1001 0000 0011 1010 binary

Number of turns = 0111 1110 binary or 126 decimal

Position within a turn = 0100 1100 1110 0111 1001 0000 0011 1010 binary or 1,290,244,154 decimal

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Counts
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
FB1.P

30240

7620

Signed32

Read Only

Position

FB2.P

30241

7621

Signed32

Read Only

Position

FB3.P

30242

7622

Signed32

Read Only

Position

FB4.P

30243

7623

Signed32

Read Only

Position

FB5.P

30244

7624

Signed32

Read Only

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.P

30240

Signed32

Read Only

Position

FB2.P

30241

Signed32

Read Only

Position

FB3.P

30242

Signed32

Read Only

Position

FB4.P

30243

Signed32

Read Only

Position

FB5.P

30244

Signed32

Read Only

Position

Related Topics

Scaled Feedback